TIDUEX5 October 2020
Inrush limiting is achieved with LM74810-Q1 by placing a capacitor to slow down the HGATE voltage ramp during power up. The capacitor value required depends on the desired inrush current value as well as the amount of output capacitance. Equation 4 shows how to calculate the capacitor value needed. In the equation, is typically being 53 µA.

Duration of the inrush current can be calculated by Equation 5.