TIDUEZ0A March 2021 – March 2022 TMS320F28P550SG , TMS320F28P550SJ , TMS320F28P559SG-Q1 , TMS320F28P559SJ-Q1
Figure 2-15 shows the schematic of the isolated Si MOSFET gate driver. As the UCC21541 gate driver used has two isolated gate drive outputs, it can drive both the devices in the half-bridge power stage of the power board. The drive current is controlled separately for turn-on and turn-off with diode controlled separate drive paths. A ferrite bead is used in the gate drive path to suppress ringing.
Figure 2-15 UCC21541 Gate Drive
Circuit