- To run this lab, make sure the
hardware is set up as shown in Figure 3-11. The 2-points calibration method is used to calibrate gain and offset
errors.
- To measure current, use an
external precision resistor and a DMM, or you can use E-Load current readings.
Alternatively, voltage across sense resistors on the TIDA-010090 boards can be
used to measure the output current. To measure voltage, use a DMM across the
buck converter output voltage and remote sense connections.
- Open the SYSCONFIG page, select
Lab 5, and set Calibration Mode to Current Calibration. Figure 3-32 shows the SYSCONFIG page setting for current calibration.
- Save the SYSCONFIG page,
and run the code.
- Open the Expression
Window.
- The output current is
updated using BT4PH_userParam_V_I_chX->ibatCal_pu parameter.
- Set the
BT4CH_userParam_chX->Relay_ON to 1 to enable the output
relay.
- Set the
BT4CH_userParam_chX->en_bool = 1.
- Set the
BT4CH_userParam_chX->ibatCal_pu to "0.05" and "0.3", and note the
output current readings.
- Update the actual output
current readings in bt4ch_gan_cal.h file.
#define BT4CH_IBAT_ACTUAL_CH1_P1_A ((float32_t)2.5)
#define BT4CH_IBAT_ACTUAL_CH1_P2_A ((float32_t)15.00)
- Repeat the steps for
channel 2, 3 and 4.
-
Open the SYSCONFIG page,
select Lab 5, and set Calibration Mode to Voltage Calibration.
Figure 3-33 shows the SYSCONFIG page setting for voltage calibration.
- Open the SYSCONFIG page, disable
the calibration mode.
- When using non-powerSuite version
of the project, Build Settings are directly modified in
solution_settings.h file. Set CALIBRATION_MODE to (1) for
current calibration, and (2) for voltage
calibration.#define LAB_NUMBER (5)
#define CHANNEL_NUMBER (5)
#define CALIBRATION_ENABLED (true)
#define CALIBRATION_MODE (1)