TIDUFB5A December 2024 – January 2026
This reference design features redundant input supplies, protected by ideal diode controllers.
This system operation is designed so that when the zone transitions to low power mode, only one of the 12V input supplies continues to deliver power to downstream loads, while the other is shut off. In this test, one 12V supply is shut off to simulate the loss of a power supply, while the second power supply is kept on. The 12V rails are monitored on an oscilloscope. Figure 3-3 shows that when supply one is shut off, the second supply continues to power the 12V rail for downstream loads without any interruption.
In a more comprehensive system, the module software must consider the load currents of all of the outputs to avoid overloading the remaining supply.
Figure 3-3 Redundant Supply Test