TIDUFE0A June 2025 – October 2025
The key power and digital interface signals are carefully routed out from the IWRL6432AOP BGA package, primarily utilizing free space near the horizontal edges and the center of the device. The absence of via-in-pad simplifies manufacturing processes and reduces PCB cost, yielding a significant cost benefit for two-layer boards.
Designing signals on a two-layer PCB poses significant challenges due to tight constraints, necessitating proper design considerations and careful routing. To preserve the Field of View (FOV) of the antenna, designers must exercise extra caution when placing tall components within the restricted radius of the IWRL6432AOP keepout area. Conversely, the BGA pads along the horizontal edges of the IWRL6432AOP facilitate efficient packing of the center and north section and south section of the package. Figure 2-7 illustrates an exemplary implementation of fan out.
Figure 2-7 TIDA-010967: IWRL6432AOP Fan
Out