TIDUFE0A June 2025 – October 2025
Complete the following steps to initialize this reference design module:
| MODE | SOP0 | MODE DESCRIPTION |
|---|---|---|
| 1 | 0 | Flashing mode: The host flashes the user application or firmware to Quad Serial Peripheral Interface (QSPI) flash |
| 2 | 1 | Functional mode: IWRL6432AOP loads the user application from QSPI flash to the internal RAM and runs the application from RAM. User configuration is sent to the device over the UART interface. |

The IWRL6432AOP radar sensor on the design module is ready for programming.
TI provides the Code Composer Studio™ software for firmware programming and debugging. See also the Code Composer Studio™ integrated development environment (IDE) user guide to get the CCSTUDIO software.
The UNIFLASH software can also be used to flash the IWRL6432AOP.
TI also provides a mmWave Software Development Kit (SDK) to flash a binary file to IWRL6432AOP. See the mmWave-L-SDK tool page to get this SDK.
Use the following steps to flash the IWRL6432AOP image file by using mmWave SDK:
\MMWAVE_L_SDK installed directory\tools\visualizer


motion_and_presence_detetion_demo_aop.release.appimage
file, which is generated with the last build in
the image file steps. Obtain this file from the
project folder, that is;
SDK installed
directory\examples\mmw_demo\motion_and_presence_detection\prebuilt_binaries\xwrL64xx-aop
After the IWRL6432AOP programming completes, unplug the USB cable to power off the radar module and switch SW1 to the Function mode.
Use the following steps to flash the IWRL6432AOP image file by using UniFlash:
Figure 3-6 UniFlash Configuration for
IWRL6432AOPmotion_and_presence_detetion_demo_aop.release.appimage
file, which is generated with the last build in
the image file steps. Obtain this file from the
project folder, that is;
SDK installed
directory\examples\mmw_demo\motion_and_presence_detection\prebuilt_binaries\xwrL64xx-aop
Figure 3-7 UniFlash Software Load Image for
IWRL6432AOP
After the IWRL6432AOP programming completes, unplug the USB cable to power off the radar module and switch SW1 to the Function mode.