TIDUFF0A December 2025 – March 2026
For systems with additional safety requirements, diagnostic and monitoring features have been included in this reference design.
Watchdog: The LP8772x-Q1 device includes a Q&A watchdog to monitor software lockup, and a system error monitoring input (nERR) with fault injection option to monitor the lock-step signal of the attached AWR2188. In this implementation, the I2C bus is used for the communication between the PMIC and the MSPM0G3519-Q1. This watchdog requires specific messages from the MSPM0 in specific time intervals to detect correct operation of the MSPM0. When the watchdog detects an incorrect operation of the MSPM0, the LP8772x-Q1 utilizes the nRESET pin to issue a hard reset to the AWR2188.
Voltage Monitors (VMON): The voltage monitoring pins within the LP8772x-Q1 have been connected to the 1V2 generated by TPS6285018A-Q1. In the event of an under voltage or over voltage event, this allows the PMIC to monitor this rail and using nRESET pin to issue a hard reset to the AWR2188. The VMON thresholds and the actions taken during an OV/UV condition are configured in the Non-Volatile Memory (NVM) settings of the PMIC, and are re-configurable over I2C.