TIDUFL1 November 2026 DRV8106-Q1 , DRV81646-Q1 , MSPM0G3519 , TCAN844-Q1 , TPS1200-Q1
Figure 1-1 shows the waveforms of the pump motor in continuous operating mode at 15Hz. Compared to the discrete mode, the peak transient current is significantly lower because the motor does not have sufficient time to decelerate between cycles; the mechanical momentum maintains a higher base speed.
Figure 4-10 Pump Motor Continuous Operation Mode
Waveforms (15Hz)Figure 4-11 shows the turn-off transient characteristics of the pump motor. When the PWM signal transitions to low, the HSS of the pump motor is turned off. The motor current is then conducted through the paralleled diode, which clamps the motor voltage to the negative diode's forward voltage VF. Once the motor current decays to zero, the diode ceases conduction, and the motor voltage becomes equal to the generated EMF, which is proportional to the motor's rotational speed.
In this reference design, the turn-on and turn-off driving strength of the DRV8106-Q1 is configured to 62mA through the SPI, as observed in the red waveform.
Figure 4-11 Pump Motor Turn OFF Waveforms