JAJSN79C December 2021 – October 2022 DRV8328
PRODUCTION DATA
In the case of device latched faults, the DRV8328 goes into a partial shutdown state to help protect the external power MOSFETs and system.
When the fault condition clears, the device can be re-enabled by issuing a reset pulse to the nSLEEP pin. The nSLEEP reset pulse (tRST) consists of a high-to-low-to-high transition on the nSLEEP pin. The reset pulse has no effect on any of the regulators, device settings, or other functional blocks as long as the low period of the sequence falls within the tRST time window. If the pulse is longer than the tRST time window, the device will start a complete shutdown sequence.