JAJSDY1C June 2017 – March 2018 TPS25740B
PRODUCTION DATA.
In applications where there are load transients or moderate ripple on VOUT, the OCP performance of TPS25740B may be impacted. Adding the RF/CF filter network as shown in Figure 48 helps mitigate the impact of the ripple and load transients on OCP performance.
RF/CF can be tailored to the amount of ripple on VOUT as shown in Table 6.
FREQUENCY x RIPPLE (kHz x V) | SUGGESTED FILTER TIME CONSTANT (µs) |
---|---|
< 5 (Ex: 50 mV ripple at 100 kHz) | None |
5 to 15 | 2.2 µs ( RF = 10 Ω, CF = 220 nF) |
15 to 35 | 4.7 µs ( RF = 10 Ω, CF = 470 nF) |
35 to 105 | 10 µs ( RF = 10 Ω, CF = 1 µF) |