8.5.2 Block Register Write
The I2C Block Register Write transaction is illustrated in Figure 11 and consists of the following sequence.
- Master issues a Start Condition.
- Master writes the 7-bit Slave Address following by a Write bit.
- Master writes the 8-bit Register address as the CommandCode of the programming sequence.
- Master writes one or more data bytes each of which should be acknowledged by the slave. The slave increments the internal register address after each byte.
- Master issues a Stop Condition to terminate the transaction.