SLUUCY9 November   2023 BQ76905

 

  1.   1
  2.   Description
  3.   Get Started
  4.   Features
  5.   Applications
  6.   6
  7. 1Evaluation Module Overview
    1. 1.1 Introduction
    2. 1.2 Kit Contents
    3. 1.3 Specification
    4. 1.4 Device Information
  8. 2Hardware
    1. 2.1 Before You Begin
    2. 2.2 Required Equipment
    3. 2.3 BQ76905 Circuit Module Use
      1. 2.3.1 Cell Simulator
      2. 2.3.2 Evaluating with Load Current
      3. 2.3.3 Evaluating Charge and Discharge Currents
      4. 2.3.4 Evaluating with Simulated Current
      5. 2.3.5 Reducing the Cell Count
      6. 2.3.6 Connecting Cells
      7. 2.3.7 Connecting to a Host
      8. 2.3.8 Hardware Configuration
        1. 2.3.8.1 Configuration Jumpers
      9. 2.3.9 Configuration Register Programming
  9. 3Quick Start Guide
  10. 4Software
    1. 4.1 Battery Management Studio Software
      1. 4.1.1 System Requirements
      2. 4.1.2 Installing BQStudio
      3. 4.1.3 BQ76905 bqz File Installation
      4. 4.1.4 BQStudio Operation and Registers View
      5. 4.1.5 Commands
      6. 4.1.6 Data Memory
        1. 4.1.6.1 Entering, Saving, and Loading Configuration
      7. 4.1.7 Command Sequences
  11. 5Hardware Design Files
    1. 5.1 Schematic
    2. 5.2 Board Layout
    3. 5.3 Bill of Materials
  12. 6Additional Information
    1.     Trademarks

BQStudio Operation and Registers View

BQStudio is used to communicate to the BQ76905 for evaluation. BQStudio includes several tools to aid in configuration, calibration and data display of the BQ76905 during evaluation.

Although the software runs without connection to an interface board or powered device, TI recommends to have the interface connected and the device on when starting the software. Follow the directions in Section 3. Figure 4-1 shows typical connections for operation with the BQStudio software.

Start the software from the desktop shortcut Battery Management Studio or from the Start menu.

When started, the software looks for the communication interface and the device. If the device is not found, then the device opens a Target Selection Wizard. On the first window select the Monitor or All class and click the Next button. On the second window select the newest or appropriate BQ76905 version in the list and click the Finish button. This selection is remembered until the software is re-started. If the device is not found, then the user is presented with a Proceed? window, which must be acknowledged. If the software still cannot find the device, then a Battery Management Studio pop-up window appears indicating communication status. Acknowledge the message to proceed.

GUID-20220708-SS0I-FKJL-RPX4-P2DNPVSPMV1D-low.pngFigure 4-1 Target Selection Wizard

If the software was started without a communication interface adapter, then a Battery Management Studio pop-up window indicates a free adapter is not available. Acknowledge the message to proceed. Errors appear in the left bottom border of the Battery Management Studio screen. Correct the problem with the adapter and restart the software.

BQStudio contains a user's guide for general operation of the software. Refer to the menu selection Help | Help Contents for information.

The BQStudio window appears as shown in Figure 5-2. The register area is blank since the device is not attached.

The center panel of BQStudio displays tool tips when the cursor is held over an item name. The tool tip provides some description of the item. The tool tip closes after approximately 30 seconds. To avoid the tool tip display move the cursor to the value or units column, or to the Dashboard panel.

GUID-20220722-SS0I-FQP7-Z7SH-GQRP0X1CTLKJ-low.pngFigure 4-2 BQStudio Window without Device

Without a device, BQStudio operates with reduced functions. Tools can be browsed and data fields inspected, but data cannot be entered.

The dashboard on the left-side of the window shows the adapter, device and simple voltage and current displays. The dashboard updates periodically unless Auto Refresh is stopped by clicking on the banner. The right side of the window has the Commands panel.

The center panel of the window initially shows the Registers tab. The register display shows device status registers and is read once when the device is detected. To update the register values select the Refresh button at the top of the Registers tab. To repeatedly read the registers select the Scan button. To repeatedly read and log the register values to a file select the Start Log button and follow the prompts to save a log file. When a log is running, select Stop Log to end the log and close the file. The Parameter View selection allows the choice of basic parameters which shows commonly used registers, or all parameters which shows more registers.

If a device is connected and powered after BQStudio is powered, then the dashboard auto-detects the device and update the device and register display. Figure 5-3 shows a register display with a connected device.

GUID-20220722-SS0I-JWQZ-LGSL-XZWQWR78PDBB-low.pngFigure 4-3 Register View with Device

The available tools for the device are shown at the top of the window and can be selected by clicking on the tool icon. Tools can also be selected from the View menu as shown in Figure 5-4. Opening a new tool can change the center tab of the window. Not all devices have all the tools described. Multiple tools can be active at one time, which use the center pane for display are shown as a tabs at the top of the center section. These tabs can be closed with the X as desired, but closing the tab can terminate the operation running in the tab.

GUID-20220722-SS0I-G6JF-T8JK-DJ8PB5C8TMHM-low.pngFigure 4-4 Tool Selections