SPNU118Z September 1995 – March 2023 66AK2E05 , 66AK2H06 , 66AK2H12 , 66AK2H14 , AM1705 , AM1707 , AM1802 , AM1806 , AM1808 , AM1810 , AM5K2E04 , C346BA02 , C348A01 , CS241C01-Q1 , CS241C05-Q1 , CS246C01-Q1 , CS348C02-Q1 , OMAP-L132 , OMAP-L137 , OMAP-L138 , S470AV336LYSQRB , TMS470R1A288 , TMS470R1A384 , TMS470R1A64 , TMS470R1B1M , TMS470R1B512 , TMS470R1B768
Linker options control linking operations. They can be placed on the command line or in a command file. Linker options must be preceded by a hyphen (-). Options can be separated from arguments (if they have them) by an optional space.
Option | Alias | Description | Section |
---|---|---|---|
--run_linker | -z | Enables linking | Section 8.3 |
--output_file | -o | Names the executable output module. The default filename is a.out. | Section 8.4.25 |
--map_file | -m | Produces a map or listing of the input and output sections, including holes, and places the listing in filename | Section 8.4.20 |
--stack_size | -stack | Sets C system stack size to size bytes and defines a global symbol that specifies the stack size. Default = 2K bytes | Section 8.4.31 |
--heap_size | -heap | Sets heap size (for the dynamic memory allocation in C) to sizebytes and defines a global symbol that specifies the heap size. Default = 2K bytes | Section 8.4.16 |
Option | Alias | Description | Section |
---|---|---|---|
--library | -l | Names an archive library or link command filename as linker input | Section 8.4.18 |
--disable_auto_rts | Disables the automatic selection of a run-time-support library | Section 8.4.9 | |
--priority | -priority | Satisfies unresolved references by the first library that contains a definition for that symbol | Section 8.4.18.3 |
--reread_libs | -x | Forces rereading of libraries, which resolves back references | Section 8.4.18.3 |
--search_path | -i | Alters library-search algorithms to look in a directory named with pathname before looking in the default location. This option must appear before the --library option. | Section 8.4.18.1 |
Option | Alias | Description | Section |
---|---|---|---|
--define | Predefines name as a preprocessor macro. | Section 8.4.11 | |
--undefine | Removes the preprocessor macro name. | Section 8.4.11 | |
--disable_pp | Disables preprocessing for command files | Section 8.4.11 |
Option | Alias | Description | Section |
---|---|---|---|
--diag_error | Categorizes the diagnostic identified by num as an error | Section 8.4.8 | |
--diag_remark | Categorizes the diagnostic identified by num as a remark | Section 8.4.8 | |
--diag_suppress | Suppresses the diagnostic identified by num | Section 8.4.8 | |
--diag_warning | Categorizes the diagnostic identified by num as a warning | Section 8.4.8 | |
--display_error_number | Displays a diagnostic's identifiers along with its text | Section 8.4.8 | |
--emit_references:file[=file] | Emits a file containing section information. The information includes section size, symbols defined, and references to symbols. | Section 8.4.8 | |
--emit_warnings_as_errors | -pdew | Treats warnings as errors | Section 8.4.8 |
--issue_remarks | Issues remarks (nonserious warnings) | Section 8.4.8 | |
--no_demangle | Disables demangling of symbol names in diagnostics | Section 8.4.22 | |
--no_warnings | Suppresses warning diagnostics (errors are still issued) | Section 8.4.8 | |
--set_error_limit | Sets the error limit to num. The linker abandons linking after this number of errors. (The default is 100.) | Section 8.4.8 | |
--verbose_diagnostics | Provides verbose diagnostics that display the original source with line-wrap | Section 8.4.8 | |
--warn_sections | -w | Displays a message when an undefined output section is created | Section 8.4.35 |
Option | Alias | Description | Section |
---|---|---|---|
--absolute_exe | -a | Produces an absolute, executable module. This is the default; if neither --absolute_exe nor --relocatable is specified, the linker acts as if --absolute_exe were specified. | Section 8.4.3.1 |
--ecc={ on | off } | Enable linker-generated Error Correcting Codes (ECC). The default is off. | Section 8.4.12 Section 8.5.9 |
|
--ecc:data_error | Inject the specified errors into the output file for testing | Section 8.4.12 Section 8.5.9 |
|
--ecc:ecc_error | Inject the specified errors into the Error Correcting Code (ECC) for testing | Section 8.4.12 Section 8.5.9 |
|
--mapfile_contents | Controls the information that appears in the map file. | Section 8.4.21 | |
--relocatable | -r | Produces a nonexecutable, relocatable output module | Section 8.4.3.2 |
--generate_dead_funcs_list | Writes a list of the dead functions that were removed by the linker to file fname. | Section 8.4.15 | |
--run_abs | -abs | Produces an absolute listing file | Section 8.4.29 |
--xml_link_info | Generates a well-formed XML file containing detailed information about the result of a link | Section 8.4.36 |
Option | Alias | Description | Section |
---|---|---|---|
--entry_point | -e | Defines a global symbol that specifies the primary entry point for the output module | Section 8.4.13 |
--globalize | Changes the symbol linkage to global for symbols that match pattern | Section 8.4.19 | |
--hide | Hides global symbols that match pattern | Section 8.4.17 | |
--localize | Changes the symbol linkage to local for symbols that match pattern | Section 8.4.19 | |
--make_global | -g | Makes symbol global (overrides -h) | Section 8.4.19.1 |
--make_static | -h | Makes all global symbols static | Section 8.4.19.1 |
--no_symtable | -s | Strips symbol table information and line number entries from the output module | Section 8.4.24 |
--retain | Retains a list of sections that otherwise would be discarded | Section 8.4.28 | |
--scan_libraries | -scanlibs | Scans all libraries for duplicate symbol definitions | Section 8.4.30 |
--symbol_map | Maps symbol references to a symbol definition of a different name | Section 8.4.32 | |
--undef_sym | -u | Places an unresolved external symbol into the output module's symbol table | Section 8.4.34 |
--unhide | Reveals (un-hides) global symbols that match pattern | Section 8.4.17 |
Option | Alias | Description | Section |
---|---|---|---|
--arg_size | --args | Allocates memory to be used by the loader to pass arguments | Section 8.4.4 |
-be32 | Forces the linker to generate BE-32 object code. | Section 8.4.5 | |
-be8 | Forces the linker to generate BE-8 object code. | Section 8.4.5 | |
--cinit_hold_wdt={on|off} | Hold (on) or do not hold (off) watchdog timer during cinit auto-initialization. | Section 8.11.5 | |
--fill_value | -f | Sets default fill values for holes within output sections; fill_value is a 32-bit constant | Section 8.4.14 |
--ram_model | -cr | Initializes variables at load time | Section 8.4.27 |
--rom_model | -c | Autoinitializes variables at run time | Section 8.4.27 |
--trampolines | Generates far call trampolines; on by default | Section 8.4.33 |
Option | Alias | Description | Section |
---|---|---|---|
--cinit_compression [=compression_kind] | Specifies the type of compression to apply to the C auto initialization data. The default if this option is used with no kind specified is lzss for Lempel-Ziv-Storer-Szymanski compression. Alternately, specify --cinit_compression=rle to use Run Length Encoded compression, which generally provides less efficient compression. | Section 8.4.6 | |
--compress_dwarf | Aggressively reduces the size of DWARF information from input object files | Section 8.4.7 | |
--copy_compression [=compression_kind] | Compresses data copied by linker copy tables | Section 8.4.6 | |
--unused_section_elimination | Eliminates sections that are not needed in the executable module; on by default | Section 8.4.10 |
Option | Alias | Description | Section |
---|---|---|---|
--linker_help | -help | Displays information about syntax and available options | – |
--minimize_trampolines | Places sections to minimize number of far trampolines required | Section 8.4.33.2 | |
--preferred_order | Prioritizes placement of functions | Section 8.4.26 | |
--trampoline_min_spacing | When trampoline reservations are spaced more closely than the specified limit, tries to make them adjacent | Section 8.4.33.3 | |
--zero_init | Controls preinitialization of uninitialized variables. Default is on.Always off if --ram_model is used. | Section 8.4.37 |