SPNU118Z September 1995 – March 2023 66AK2E05 , 66AK2H06 , 66AK2H12 , 66AK2H14 , AM1705 , AM1707 , AM1802 , AM1806 , AM1808 , AM1810 , AM5K2E04 , C346BA02 , C348A01 , CS241C01-Q1 , CS241C05-Q1 , CS246C01-Q1 , CS348C02-Q1 , OMAP-L132 , OMAP-L137 , OMAP-L138 , S470AV336LYSQRB , TMS470R1A288 , TMS470R1A384 , TMS470R1A64 , TMS470R1B1M , TMS470R1B512 , TMS470R1B768
To invoke the hex conversion utility, enter:
armhex [options] filename |
armhex | is the command that invokes the hex conversion utility. |
options | supplies additional information that controls the hex conversion process. You can use options on the command line or in a command file. Table 12-1 lists the basic options.
|
filename | names an object file or a command file (for more information, see Section 12.2.2). |
Option | Alias | Description | See |
---|---|---|---|
General Options | |||
--byte | -byte | Number output locations by bytes rather than by target addressing | -- |
--entrypoint=addr | -e | Specify the entry point at which to begin execution after boot loading | Section 12.11.3 |
--exclude={fname(sname) | sname} |
-exclude | If the filename (fname) is omitted, all sections matching sname will be excluded. | Section 12.7 |
--fill=value | -fill | Fill holes with value | Section 12.9.2 |
--help | -options, -h | Display the syntax for invoking the utility and list available options. If the option is followed by another option or phrase, detailed information about that option or phrase is displayed. | Section 12.2.2 |
--image | -image | Select image mode | Section 12.9.1 |
--linkerfill | -linkerfill | Include linker fill sections in images | -- |
--map=filename | -map | Generate a map file | Section 12.4.2 |
--memwidth=value | -memwidth | Define the system memory word width (default 16 bits) | Section 12.3.2 |
--outfile=filename | -o | Specify an output filename | Section 12.8 |
--quiet | -q | Run quietly (when used, it must appear before other options) | Section 12.2.2 |
--romwidth=value | -romwidth | Specify the ROM device width (default depends on format used). This option is ignored for the TI-TXT, binary, and TI-Tagged formats. | Section 12.3.3 |
--zero | -zero, -z | Reset the address origin to 0 in image mode | Section 12.9.3 |
Diagnostic Options | |||
--diag_error=id | Categorizes the diagnostic identified by id as an error | Section 12.14 | |
--diag_remark=id | Categorizes the diagnostic identified by id as a remark | Section 12.14 | |
--diag_suppress=id | Suppresses the diagnostic identified by id | Section 12.14 | |
--diag_warning=id | Categorizes the diagnostic identified by id as a warning | Section 12.14 | |
--display_error_number | Displays a diagnostic's identifiers along with its text | Section 12.14 | |
--issue_remarks | Issues remarks (nonserious warnings) | Section 12.14 | |
--no_warnings | Suppresses warning diagnostics (errors are still issued) | Section 12.14 | |
--set_error_limit=count | Sets the error limit to count. The linker abandons linking after this number of errors. (The default is 100.) | Section 12.14 | |
Boot Options | |||
--cmac=file | Specify a file containing the CMAC key for use with secure flash boot on TMS320F2838x devices. | Section 12.12 | |
Output Options | |||
--array | Select array output format | Section 12.10 | |
--ascii | -a | Select ASCII-Hex | Section 12.15.1 |
--binary | -b | Select binary (Must have memory width of 8 bits.) | -- |
--intel | -i | Select Intel | Section 12.15.2 |
--motorola=1 | -m1 | Select Motorola-S1 | Section 12.15.3 |
--motorola=2 | -m2 | Select Motorola-S2 | Section 12.15.3 |
--motorola=3 | -m3 | Select Motorola-S3 (default -m option) | Section 12.15.3 |
--tektronix | -x | Select Tektronix (default format if no output option specified) | Section 12.15.4 |
--ti_tagged | -t | Select TI-Tagged (Must have memory width of 16 bits.) | Section 12.15.5 |
--ti_txt | Select TI-Txt (Must have memory width of 8 bits.) | Section 12.15.6 | |
Load Image Options | |||
--load_image | Output a file with load image object format | Section 12.6 | |
--load_image:combine_sections =[true|false] | Specify whether sections should be combined. The default is true. | Section 12.6 | |
--load_image:endian=[big|little] | Specify the object file endianness. If this option is omitted, the endianness of the first file on the command line is used. | Section 12.6 | |
--load_image:file_type =[relocatable|executable] | Specify a file type other than object files. Object files can be linked with one another, but addresses are lost. Relocatable files contain the address in the sh_addr field of a section. Executable files maintain address bindings and can be directly loaded. | Section 12.6 | |
--load_image:format=[coff|elf] | Specify the ABI format of the object file. If this option is omitted, the format is determined from the first file on the command line. | Section 12.6 | |
--load_image:globalize=string | Do not localize the specified symbol. The default can be set with the --load_image:symbol_binding option. | Section 12.6 | |
--load_image:localize=string | Make the specified symbol local. The default can be set with the --load_image:symbol_binding option. | Section 12.6 | |
--load_image:machine=[ARM| C2000|C6000|C7X|MSP430|PRU] | Specify the object file machine type. If this option is omitted, the machine type from the first file on the command line is used. | Section 12.6 | |
--load_image:output_symbols =[true|false] | Specify whether symbols should be output to the file. The default is false. | Section 12.6 | |
--load_image:section_addresses =[true|false] | Specify whether the load address should be written in the output file. Applies to relocatable files only. The default is true. | Section 12.6 | |
--load_image:section_prefix =string | Specify a prefix for section names. The default is "image_". | Section 12.6 | |
--load_image:symbol_binding =[local|global] | Specify the default binding of symbols in the load image. | Section 12.6 |
The --section_name_prefix option is deprecated and replaced by --load_image:section_prefix. Undocumented --host_image options have been replaced with --load_image options that are similar in many cases.