SPNU118Z September 1995 – March 2023 66AK2E05 , 66AK2H06 , 66AK2H12 , 66AK2H14 , AM1705 , AM1707 , AM1802 , AM1806 , AM1808 , AM1810 , AM5K2E04 , C346BA02 , C348A01 , CS241C01-Q1 , CS241C05-Q1 , CS246C01-Q1 , CS348C02-Q1 , OMAP-L132 , OMAP-L137 , OMAP-L138 , S470AV336LYSQRB , TMS470R1A288 , TMS470R1A384 , TMS470R1A64 , TMS470R1B1M , TMS470R1B512 , TMS470R1B768
These terms defined appear in the cross-reference listing in Cross-Reference Listing:
Symbol | Name of the symbol listed | |
Filename | Name of the file where the symbol appears | |
RTYP | The symbol's reference type in this file. The possible reference types are: | |
STAT | The symbol is defined in this file and is not declared as global. | |
EDEF | The symbol is defined in this file and is declared as global. | |
EREF | The symbol is not defined in this file but is referenced as global. | |
UNDF | The symbol is not defined in this file and is not declared as global. | |
AsmVal | This hexadecimal number is the value assigned to the symbol at assembly time. A value may also be preceded by a character that describes the symbol's attributes. Table 10-1 lists these characters and names. | |
LnkVal | This hexadecimal number is the value assigned to the symbol after linking. | |
DefLn | The statement number where the symbol is defined. | |
RefLn | The line number where the symbol is referenced. If the line number is followed by an asterisk (*), then that reference can modify the contents of the object. A blank in this column indicates that the symbol was never used. |
Character | Meaning |
---|---|
' | Symbol defined in a .text section |
" | Symbol defined in a .data section |
+ | Symbol defined in a .sect section |
- | Symbol defined in a .bss or .usect section |
Cross-Reference Listing is an example of cross-reference listing.
File: bttest.out Wed Nov 13 17:07:42 xxxxPage: 1
=============================================================================
Symbol: array
Filename RTYP AsmVal LnkVal DefLn RefLn RefLn RefLn
________ ____ ________ ________ ______ _______ _______ _______
module1.asm EDEF -00000001 00001001 3 1A 5
=============================================================================
Symbol: array_a
Filename RTYP AsmVal LnkVal DefLn RefLn RefLn RefLn
________ ____ ________ ________ ______ _______ _______ _______
module1.asm STAT '00000004 00000004 5 9
=============================================================================
Symbol: dflag
Filename RTYP AsmVal LnkVal DefLn RefLn RefLn RefLn
________ ____ ________ ________ ______ _______ _______ _______
module1.asm EDEF -00000000 00001000 2 3A 4
=============================================================================
Symbol: dflag_a
Filename RTYP AsmVal LnkVal DefLn RefLn RefLn RefLn
________ ____ ________ ________ ______ _______ _______ _______
module1.asm STAT '00000000 00000000 4 11
=============================================================================
Symbol: offst
Filename RTYP AsmVal LnkVal DefLn RefLn RefLn RefLn
________ ____ ________ ________ ______ _______ _______ _______
module1.asm EREF 00000000 00001068 2A 6
module2.asm EDEF -00000000 00001068 2 2A 3
=============================================================================
Symbol: offst_a
Filename RTYP AsmVal LnkVal DefLn RefLn RefLn RefLn
________ ____ ________ ________ ______ _______ _______ _______
module1.asm STAT '00000008 00000008 6 10
module2.asm STAT '00000000 00000020 3 6
=============================================================================