SPNU118Z September 1995 – March 2023 66AK2E05 , 66AK2H06 , 66AK2H12 , 66AK2H14 , AM1705 , AM1707 , AM1802 , AM1806 , AM1808 , AM1810 , AM5K2E04 , C346BA02 , C348A01 , CS241C01-Q1 , CS241C05-Q1 , CS246C01-Q1 , CS348C02-Q1 , OMAP-L132 , OMAP-L137 , OMAP-L138 , S470AV336LYSQRB , TMS470R1A288 , TMS470R1A384 , TMS470R1A64 , TMS470R1B1M , TMS470R1B512 , TMS470R1B768
Define Macro
macname .macro [parameter1[, ... ,parametern]]
model statements or macro directives
.endm
The .macro and .endm directives are used to define macros.
You can define a macro anywhere in your program, but you must define the macro before you can use it. Macros can be defined at the beginning of a source file, in an .include/.copy file, or in a macro library.
macname | names the macro. You must place the name in the source statement's label field. | |
.macro | identifies the source statement as the first line of a macro definition. You must place .macro in the opcode field. | |
[parameters] | are optional substitution symbols that appear as operands for the .macro directive. | |
model statements | are instructions or assembler directives that are executed each time the macro is called. | |
macro directives | are used to control macro expansion. | |
.endm | marks the end of the macro definition. |
Macros are explained in further detail in Chapter 177.