SPNU118Z September 1995 – March 2023 66AK2E05 , 66AK2H06 , 66AK2H12 , 66AK2H14 , AM1705 , AM1707 , AM1802 , AM1806 , AM1808 , AM1810 , AM5K2E04 , C346BA02 , C348A01 , CS241C01-Q1 , CS241C05-Q1 , CS246C01-Q1 , CS348C02-Q1 , OMAP-L132 , OMAP-L137 , OMAP-L138 , S470AV336LYSQRB , TMS470R1A288 , TMS470R1A384 , TMS470R1A64 , TMS470R1B1M , TMS470R1B512 , TMS470R1B768
Define Messages
.emsg string
.mmsg string
.wmsg string
These directives allow you to define your own error and warning messages. When you use these directives, the assembler tracks the number of errors and warnings it encounters and prints these numbers on the last line of the listing file.
The .emsg directive sends an error message to the standard output device in the same manner as the assembler. It increments the error count and prevents the assembler from producing an object file.
The .mmsg directive sends an assembly-time message to the standard output device in the same manner as the .emsg and .wmsg directives. It does not, however, set the error or warning counts, and it does not prevent the assembler from producing an object file.
The .wmsg directive sends a warning message to the standard output device in the same manner as the .emsg directive. It increments the warning count rather than the error count, however. It does not prevent the assembler from producing an object file.
This example sends the message ERROR -- MISSING PARAMETER to the standard output device.
Source file:
MSG_EX .macro parm1
.if $$symlen(parm1) = 0
.emsg "ERROR -- MISSING PARAMETER"
.else
ADD parm1, r7, r8
.endif
.endm
MSG_EX R0
MSG_EX
Listing file:
1 MSG_EX .macro parm1
2 .if $$symlen(parm1) = 0
3 .emsg "ERROR -- MISSING PARAMETER"
4 .else
5 ADD parm1, r7, r8
6 .endif
7 .endm
8
9 00000000 MSG_EX R0
1 .if $$symlen(parm1) = 0
1 .emsg "ERROR -- MISSING PARAMETER"
1 .else
1 00000000 E0870008 ADD R0, r7, r8
1 .endif
10
11 00000004 MSG_EX
1 .if $$symlen(parm1) = 0
1 .emsg "ERROR -- MISSING PARAMETER"
***** USER ERROR ***** - : ERROR -- MISSING PARAMETER
1 .else
1 ADD parm1, r7, r8
1 .endif
1 Error, No Warnings
In addition, the following messages are sent to standard output by the assembler:
*** ERROR! line 11: ***** USER ERROR ***** - : ERROR -- MISSING PARAMETER
.emsg "ERROR -- MISSING PARAMETER" ]]
1 Error, No Warnings
Errors in source - Assembler Aborted