SPNU118Z September 1995 – March 2023 66AK2E05 , 66AK2H06 , 66AK2H12 , 66AK2H14 , AM1705 , AM1707 , AM1802 , AM1806 , AM1808 , AM1810 , AM5K2E04 , C346BA02 , C348A01 , CS241C01-Q1 , CS241C05-Q1 , CS246C01-Q1 , CS348C02-Q1 , OMAP-L132 , OMAP-L137 , OMAP-L138 , S470AV336LYSQRB , TMS470R1A288 , TMS470R1A384 , TMS470R1A64 , TMS470R1B1M , TMS470R1B512 , TMS470R1B768
By default, the linker does not compress copy table (Section 3.3.3 and Section 8.8) source data sections. The --cinit_compression and --copy_compression options specify compression through the linker.
The --cinit_compression option specifies the compression type the linker applies to the C autoinitialization copy table source data sections. The default is lzss.
Overlays can be managed by using linker-generated copy tables. To save ROM space the linker can compress the data copied by the copy tables. The compressed data is decompressed during copy. The --copy_compression option controls the compression of the copy data tables.
The syntax for the options are:
--cinit_compression[=compression_kind]
--copy_compression[=compression_kind]
The compression_kind can be one of the following types:
Compressed sections within initialization tables are byte aligned in order to reduce the occurrence of holes in the .cinit table.
See Section 8.8.5 for more information about compression.