SWRA770 august 2023 CC2564C
The DisplayInquiryList command exists to display the current Inquiry List with indexes. This command is useful for when a user has forgotten the Inquiry Index for a particular Bluetooth Device the user wants to interact with. This function returns zero on a successful execution and a negative value on all errors. The command requires that a valid BluetoothStack ID exists before running and must be called after using the Inquiry command, since the list is empty without already discovering devices.
Including parameters is not necessary when using this command. A parameter has no effect on the outcome of the Inquiry List displayed.