SWRA770 august 2023 CC2564C
Initiating a connection from the HID Device is the same as the procedure as the Host except that we run the inquiry (mentioned above in Step 3 of Device 1) on the HID Device instead and issue a ConnectRemoteHIDHost <Inquiry Index> where the Inquiry Index is the number that corresponds to the BD-ADDR of the Host when we run the inquiry.