SWRA770 august   2023 CC2564C

 

  1.   1
  2.   Abstract
  3.   Trademarks
  4. 1Demo Overview
  5. 2Running the Bluetooth Code
  6. 3Demo Application
    1. 3.1 Device 1 (Host/HID Host) Setup on the Demo Application
    2. 3.2 Device 2 (Client/HID Device Setup on the Demo Application
    3. 3.3 Initiating Connection from the HID Host
    4. 3.4 Initiating Connection from HID Device
    5. 3.5 Communication Between Host and Device
  7. 4Application Commands
  8. 5Gap Commands
    1. 5.1  Help (DisplayHelp)
    2. 5.2  Inquiry
    3. 5.3  Display Inquiry List
    4. 5.4  Pair
    5. 5.5  End Pairing
    6. 5.6  PIN Code Response
    7. 5.7  Pass Key Response
    8. 5.8  User Confirmation Response
    9. 5.9  Set Discoverability Mode
    10. 5.10 Set Connectability Mode
    11. 5.11 Set Pairability Mode
    12. 5.12 Change Simple Pairing Parameters
    13. 5.13 Get Local Address
    14. 5.14 Set Local Name
    15. 5.15 Get Local Name
    16. 5.16 Set Class of Device
    17. 5.17 Get Class of Device
    18. 5.18 Get Remote Name
  9. 6Human Interface Demo Profile
    1. 6.1 Host
      1. 6.1.1  Connect Remote HID Device
      2. 6.1.2  Close Connection
      3. 6.1.3  Control Request
      4. 6.1.4  Get Report Request
      5. 6.1.5  Set Report Request
      6. 6.1.6  Get Protocol Request
      7. 6.1.7  Set Protocol Request
      8. 6.1.8  Get Idle Request
      9. 6.1.9  Set Idle Request
      10. 6.1.10 Data Write
    2. 6.2 Client
      1. 6.2.1 Get Report Response
      2. 6.2.2 Set Report Response
      3. 6.2.3 Get Protocol Response
      4. 6.2.4 Set Protocol Response
      5. 6.2.5 Get Idle Response
      6. 6.2.6 Set Idle Response
  10. 7References
  11. 8Revision History

Get Idle Response

Description

The following function is responsible for sending a response for an outstanding GET_IDLE Transaction to the remote HID Host. This function returns zero on successful execution and a negative value on all errors.

Parameters

GetIdleResponse requires two parameters, ResultType, 0= rtSuccessful, 1= rtNotReady, 2= rtErrInvalidReportID, 3= rtErrUnsupportedRequest, 4= rtErrInvalidParameter, 5=rtErrUnknown, 6= rtErrFatal, 7= rtData and IdleRate.

Possible Return Values

  • (0) HID_Set_Idle_Response: Function Successful
  • (-4) FUNCTION_ERROR
  • (-6)INVALID_PARAMETERS_ERROR
  • (-8) INVALID_STACK_ID_ERROR
  • (-103)BTPS_ERROR_FEATURE_NOT_AVAILABLE
  • (-1000)BTHID_ERROR_INVALID_PARAMETER
  • (-1001)BTHID_ERROR_NOT_INITIALIZED
  • (-1002)BTHID_ERROR_INVALID_BLUETOOTH_STACK_ID
  • (-1005)BTHID_ERROR_INVALID_OPERATION

API Call

HID_Get_Idle_Response(BluetoothStackID, HIDID, (HID_Result_Type_t)TempParam->Params[0].intParam, (Byte_t)TempParam->Params[1].intParam)

API Prototype

int BTPSAPI HID_Get_Idle_Response(unsigned int BluetoothStackID, unsigned int HIDID, HID_Result_Type_t ResultType, Byte_t IdleRate)

Description of API

The following function is responsible for sending the appropriate Response to an outstanding GET_IDLE transaction. This function accepts the Bluetooth Stack ID of the BluetoothStack which is to send the response and the HID ID for which the connection has been established. The third parameter to this function is the Result Type that is to be associated with this response. The rtSuccessful Result Type is invalid for use with this function. If the rtNotReady through rtErrFatal Result Types are specified, then this function responds to the GET_IDLE Transaction with a HANDSHAKE response that has a Result Code parameter of the specified error condition. If the ResultType specified is rtData the GET_IDLEtransaction is responded to with a DATA Response that has the Idle Rate specified as the final parameter as the payload. This function returns zero if successful, or a negative return error code if there was an error.