SWRA770 august 2023 CC2564C
The GetClassOfDevice command is responsible for querying the Bluetooth Class of Device of the local Bluetooth Device. This function returns zero on a successful execution and anegative value on all errors. A Bluetooth Stack ID must exist before attempting to call this function.
Including parameters is not necessary when using this command. A parameter has no effect on the outcome of the query.
GAP_Query_Class_Of_Device(BluetoothStackID, &Class_of_Device)
int BTPSAPI GAP_Query_Class_Of_Device(unsigned int BluetoothStackID, Class_of_Device_t *Class_of_Device)
This function is responsible for querying (and reporting) the class of device of the local Bluetooth Device. The second parameter is a pointer to a class of device buffer that is to receive the Bluetooth class of device of the local device. If this function is successful, this function returns zero, and the buffer that Class_Of_Device points to is filled with the class of device read from the local Bluetooth Device. If there is an error, this function returns a negative value, and the class of device of the local Bluetooth Device is NOT copied into the specified input buffer.