TIDUCL0 January 2017
When paralleling FETs, current sharing becomes very important. All the parallel FETs are expected to carry equal current so that the losses are equally distributed. The FET operation can be split into conduction phase and switching phase. The effect of various parameters effecting current sharing in each of these phases is described in the following subsections.