TIDUCL0 January 2017
Figure 37 shows the motor winding current and winding voltage waveforms at a 18-V DC input and a 48.2-ARMS winding current, with a heat sink and 200LFM airflow. The result is tabulated in Table 8. The testing is done at a 95% duty cycle. Figure 38 shows the steady state thermal image of the board at the same condition, captured after 10 minutes of continuous running. The maximum FET temperature observed is 86.2°C.
VDC (V) | IDC (A) | WINDING CURRENT (RMS) (A) | DUTY CYCLE | INPUT POWER (W) |
---|---|---|---|---|
18 | 56 | 48.2 | 95% | 1008 |