SNAS852 june 2023 CDCE6214Q1TM
PRODUCTION DATA
The bit fields ch{x}_glitchless_en can be used to enable glitchless output divider update. This feature ensures that the high pulse of a clock period is not cut off by the output divider update process. It also ensures that setup and hold time of a receiver is not violated. The low pulse in the transition from earlier period to the new period is extended accordingly.
Figure 10-8 Glitchless Divider Update