SNAS810B May 2020 – December 2025 LMK5B12204
PRODUCTION DATA
Table 8-12 summarizes the address of several user-programmable bytes in EEPROM. These bytes can only be written using the SRAM direct write method prior to programming the EEPROM. Modifying these bytes from the factory default settings is optional.
| SRAM/EEPROM ADDRESS BYTE # (DECIMAL) | FIELD NAME | DESCRIPTION |
|---|---|---|
| 10 | I2C_ADDR[7:0] | I2C Target Address MSB Bits [7:3]. Bits [7:3] can be written to set the five MSBs of the 7-bit peripheral address. Bits [2:0] must be written with zeros. The two LSBs of the 7-bit address are determined by the control pins on device start-up. Default I2C_ADDR[7:0] value = 0xC8 (corresponds to 7-bit address of 0x64). Modify the value in EEPROM using SRAM direct write method. At subsequent POR cycle, the I2C_ADDR value stored in EEPROM can be read back from the read-only register, R10. |
| 11 | EEREV[7:0] | EEPROM Image Revision. This byte can be written to set the EEPROM image revision number or any customer-specific data for part traceability. Modify the value in EEPROM using SRAM direct write method. At subsequent POR cycle, the EEREV value stored in EEPROM can be read back from the read-only register, R11. |
| 249 | NVM_SPARE_BY0[7:0] | NVM Spare Bytes. These four bytes can be written with any customer-specific data for part traceability. Modify the value in EEPROM using SRAM direct write method. At subsequent POR cycle, these bytes can only be read directly from EEPROM, as there is no register allocation (see Read EEPROM). |
| 250 | NVM_SPARE_BY1[7:0] | |
| 251 | NVM_SPARE_BY2[7:0] | |
| 252 | NVM_SPARE_BY3[7:0] |