SNVS829F March 1999 – May 2026 LMP8480 , LMP8481
PRODUCTION DATA
Take care if the output is driving an A/D input with a maximum A/D maximum input voltage lower than the amplifier supply voltage because the output can swing higher than the planned load maximum resulting from input transients or shorts on the load and overload or possibly damage the A/D input.
A resistive attenuator, as shown in Figure 8-5, can be used to match the maximum swing to the input range of the A/D converter.
Figure 8-5 Typical Application With Resistive Divider Example