SNVS829F March 1999 – May 2026 LMP8480 , LMP8481
PRODUCTION DATA
For mid-range operation, VREFB must be tied to ground and VREFA can be tied to VCC or an external A/D reference voltage. The output is set to one-half the reference voltage. For example, a 5-V reference results in a 2.5-V output zero reference.
Figure 7-9 Applying a Divided Reference VoltageWhen the reference pins are biased at different voltages, the output is referenced to the average of the two applied voltages.
The reference pins must always be driven from clean, stable sources, such as A/D reference lines or clean supply lines. Any noise or drifts on the reference inputs are directly reflected in the output. Take care if the power supply is used as the reference source so as to not introduce supply noise, drift or sags into the measurement.
Different resistor divider ratios can be set by adding external resistors in series with the internal 100-kΩ resistors, though the temperature coefficient (tempco) of the external resistors may not tightly track the internal resistors and there are slight errors over temperature.
The LMP8480 is identical to the LMP8481, except that both the VREF pins are grounded internally. The LMP8481 can replace the LMP8480 if both VREF pins are grounded.