SNAS739E June 2018 – December 2025 LMX2615-SP
PRODUCTION DATA
The SYNC pin allows one to synchronize the LMX2615-SP such that the delay from the rising edge of the OSCin signal to the output signal is deterministic. Initially, the devices are locked to the input, but are not synchronized. The user sends a synchronization pulse that is reclocked to the next rising edge of the OSCin pulse. After a given time, t1, the phase relationship from OSCin to fOUT is deterministic. This time is dominated by the sum of the VCO calibration time, the analog setting time of the PLL loop, and the MASH_RST_COUNT if used in fractional mode.
When SYNC mode is enabled (VCO_PHASE_SYNC = 1), part of the channel divider (IncludedDivide) can be included in the feedback path. When IncludedDivide is not equal to 1:
| OUTx_MUX | CHANNEL DIVIDER | IncludedDivide |
|---|---|---|
| OUTA_MUX = OUTB_MUX = 1 ("VCO") | Don't Care | 1 (bypassed) |
| All other valid conditions | Divisible by 3 | SEG0 × SEG1 = 6 |
| All other values | SEG0 × SEG1 = 4 |