SCDS384B September 2018 – August 2025 TMUX6119
PRODUCTION DATA
Channel-to-channel crosstalk is defined as the voltage at the source pin (SA or SB) of an off-channel, when a 1-VRMS signal is applied at the source pin of an on-channel. Figure 7-10 shows the setup used to measure, and Equation 3 is the equation used to compute channel-to-channel crosstalk.
Figure 7-10 Channel-to-Channel Crosstalk Measurement Setup