SCDS482A February 2025 – April 2025 TMUX8612
PRODUCTION DATA
The On-Resistance of the TMUX861x is the ohmic resistance across the source (Sx) and drain (Dx) pins of the device. The On-Resistance varies with input voltage and supply voltage. The symbol RON is used to denote On-Resistance. Figure 7-1 shows the measurement setup used to measure RON. ΔRON represents the difference between the RON of any two channels, while RON_FLAT denotes the flatness that is defined as the difference between the maximum and minimum value of On-Resistance measured over the specified analog signal range.
Figure 7-1 On-Resistance Measurement Setup