SLVSH72 December 2023 TPS281C100
PRODUCTION DATA
Refer to the PDF data sheet for device specific package drawings
A high-accuracy current limit allows higher reliability, which protects the power supply during short circuit or power up. Also, it can save system costs by reducing PCB traces, connector size, and the capacity of the preceding power stage.
Current limit offers protection from overstressing to the load and integrated power FET. Current limit holds the current at the set value, and pulls up the SNS pin to VSNSFH and asserts the FAULT pin as diagnostic reports. The two current-limit thresholds are:
Additionally this value can be dynamically changed by changing the resistance on the ILIM pin. This can be seen in the Applications Section.
Both the internal current limit (Ilim,nom) and external programmable current limit are always active when VS is powered and EN is high. The lower value one (of ILIM and the external programmable current limit) is applied as the actual current limit. The typical deglitch time for the current limit to assert is 2.5µs.
Note that if a GND network is used (which leads to the level shift between the device GND and board GND), the ILIM pin must be connected with device GND. Calculate RLIM from the typical ICL value desired with Equation 2.
The RILIM value calculated here will correspond to a typical value of the current limit. For the RILIM value listed in the data sheet, the min and max current limit values are given in the electrical characteristic table. For any RILIM values in between, linear interpolation can be used to estimate the min and max values.
The minimum value for the current limit listed in the electrical characteristic table includes the variation for FAULT assertion. When designing the module to ensure the FAULT signal is not asserted during nominal operation, the minimum current limit needs to be above the nominal operation current. An example is given in Section 9.2.2.1.
For better protection from a hard short-to-GND condition (when VS and input are high and a short to GND happens suddenly), an open-loop fast-response behavior is set to turn off the channel, before the current-limit closed loop is set up. With this fast response, the device can achieve better inrush-suppression performance.