JAJSP77A November 2019 – August 2020 BQ79600-Q1
PRODUCTION DATA
UART transmitter is configurable to wait a specified number of bit periods after the last bit reception of Single Device read command frame from host before starting transmitting Response Frame using the TX_HOLD_OFF register, as showed in Figure 7-11. This provides time for the host to switch the bus direction at the end of its transmission.
Host does not need to configure register TX_HOLD_OFF in BQ79600-Q1 if Stack Read command is used. Host shall not use Broadcast Read Command.