JAJSHI5G august 2012 – april 2023 DLP7000
PRODUCTION DATA
The DLP7000 has only one functional mode, it is set to be highly optimized for low latency and high speed in generating mirror clocking pulses and timings.
When operated with the DLPC410 controller in conjunction with the DLPA200 driver, the DLP7000 can be operated in several display modes. The DLP7000 is loaded as 16 blocks of 48 rows each. Figure 8-6, Figure 8-7, Figure 8-8, and Figure 8-9 show how the image is loaded by the different Micromirror Clocking Pulse modes.
There are four Micromirror Clocking Pulse modes that determine which blocks are "reset" when a Micromirror Clocking Pulse command is issued: