JAJSMF0B July 2021 – February 2024 LMX1204
PRODUCTION DATA
The clock multiplier can be used to multiply up the input clock frequency by a factor of ×1, ×2, ×3, or ×4. The multiply value is set by the CLK_MULT field. As the multiplier is PLL-based and includes an integrated VCO, the multiplier has a state machine clock, requires calibration, has a lock detect feature, and can be used as a tunable filter. Note that if the multiplier is not being used, there is no need for the state machine clock or the lock detect feature.