JAJSM07C November 2019 – March 2022 LMX2694-SEP
PRODUCTION DATA
Table 7-17 shows the function modes of the LMX2694-SEP.
| MODE | DESCRIPTION | SOFTWARE SETTINGS |
|---|---|---|
| RESET | Registers are held in their reset state. This device does have a power-on reset, but it is good practice to also do a software reset if there is any possibility of noise on the programming lines, especially if there is sharing with other devices. Also realize that there are registers not disclosed in the data sheet that are reset as well. | RESET = 1 POWERDOWN = 0 |
| POWERDOWN | Device is powered down. | POWERDOWN = 1 |
| Normal operating mode | This is used with at least one output on as a frequency synthesizer and the device can be controlled through the SPI interface. | |
| SYNC mode | This is used where part of the channel divider is in the feedback path to ensure deterministic phase. | VCO_PHASE_SYNC = 1 |
| SYSREF mode | In this mode, RFOUTB is used to generate pulses for SYSREF. | VCO_PHASE_SYNC =1 SYSREF_EN = 1 |