JAJSLG1A april 2021 – february 2023 TDES954
PRODUCTION DATA
RX port specific register. The V3Link Port Select register 0x4C configures which unique RX port registers can be accessed by I2C read and write commands.
BIT | FIELD | TYPE | DEFAULT | DESCRIPTION |
---|---|---|---|---|
7 | RESERVED | R | 0x0 | Reserved |
6 | RX_PORT_NUM | R | 0x0 | RX Port Number. This read-only field indicates the number of the currently selected RX read port. |
5 | BCC_CRC_ERROR | R/RC | 0x0 | Bi-directional Control Channel CRC Error Detected This bit indicates a CRC error has been detected in the forward control channel. If this bit is set, an error may have occurred in the control channel operation. This bit is cleared on read. |
4 | LOCK_STS_CHG | R/RC | 0x0 | Lock Status Changed This bit is set if a change in receiver lock status has been detected since the last read of this register. Current lock status is available in the LOCK_STS bit of this register. This bit is cleared on read. |
3 | BCC_SEQ_ERROR | R/RC | 0x0 | Bi-directional Control Channel Sequence Error Detected This bit indicates a sequence error has been detected in the forward control channel. If this bit is set, an error may have occurred in the control channel operation. This bit is cleared on read. |
2 | PARITY_ERROR | R | 0x0 | V3Link parity errors detected This flag is set when the number of parity errors detected is greater than the threshold programmed in the PAR_ERR_THOLD registers. 1: Number of V3Link parity errors detected is greater than the threshold 0: Number of V3Link parity errors is below the threshold This bit is cleared when the RX_PAR_ERR_HI/LO registers are cleared. |
1 | PORT_PASS | R | 0x0 | Receiver PASS indication. This bit indicates the current status of the Receiver PASS indication. The requirements for setting the Receiver PASS indication are controlled by the PORT_PASS_CTL register. 1: Receive input has met PASS criteria 0: Receive input does not meet PASS criteria |
0 | LOCK_STS | R | 0x0 | V3Link receiver is locked to incoming data 1: Receiver is locked to incoming data 0: Receiver is not locked |