JAJSFM9A June 2018 – July 2018 TMS320F28035-EP
PRODUCTION DATA.
When the emulator is connected, the GPIO37/TDO pin cannot be used for boot mode selection. In this case, the boot ROM detects that an emulator is connected and uses the contents of two reserved SARAM locations in the PIE vector table to determine the boot mode. If the content of either location is invalid, then the Wait boot option is used. All boot mode options can be accessed in emulation boot.