JAJSNJ1H May 2013 – December 2021 TPS65310A-Q1
PRODUCTION DATA
TESTSTART mode is entered:
In this mode the OV/UV comparators of BUCK1-3, BOOST, LDO and VIO are tested. The test is implemented in such a way that during this mode all comparators have to deliver a 1 (fail condition). If this is the case the device enters TESTSTOP mode.
If this is not the case, the device stays in TESTSTART. If the WAKE pin is low, the device enters LPM0 after ttimeout. If the WAKE pin is high, the part stays in TESTSTART.