JAJSNQ5 may 2023 TPS92629-Q1
PRODUCTION DATA
The TPS92629-Q1 device is a high-side current driver for driving LEDs. The device controls each output current through regulating the voltage drop on an external high-side current-sense resistor, R(SNS). An integrated error amplifier drives an internal power transistor to maintain the voltage drop on the current-sense resistor R(SNS) to V(CS_REG) and therefore regulates the current output to target value. When the output current is in regulation, the current value for each channel can be calculated by using Equation 1.
where
When the supply voltage drops below total LED string forward voltage plus required headroom voltage, the sum of V(DROPOUT) and V(CS_REG), the TPS92629-Q1 is not able to deliver enough current output as set by the value of R(SNS), and the voltage across the current-sense resistor R(SNS) is less than V(CS_REG).