SBOU180B november 2016 – july 2023 INA260
The Registers tool (as shown in Figure 4-8) allows the user to monitor and even change the contents of the internal user-accessible registers of the INA260 on a bit-by-bit basis. Bit names for the selected register are displayed on the lower panel of the page, but the user is advised to consult the INA260 data sheet for detailed bit definitions that may be necessary when modifying the contents of the input registers.