SLAU958A January 2025 – March 2025 MSPM0G3507
The following items are required to use this tuning guide:
Figure 2-1 shows the block diagram connections for a sensorless FOC motor system. The system can be built using:
The following sections describe how to configure the pins for each portion of the sensorless FOC block diagram.
The System Configuration tool (SysConfig) helps to configure the pins in a motor control system. The default pin configurations are provided for the EVM hardware setup to spin a motor, but pins can be remapped to other pins visually inside SysConfig. This is useful for reconfiguring different pins (such as PWM, ADC, or other control signals) on a custom PCB or for scaling to different packages across MSPM0 devices.