These instructions refer to pages and
register addresses. When an I2C serial interface is used, the pages are
delineated by distinct I2C addresses while in SPI the page information is
included in the second byte of the transmission payload. The serial interface can be
changed as part of the NVM configuration as discussed in Section 5. See the device data sheet regarding page implementation.
- Unlocking the NVM
Unlocking the NVM requires a series of write
accesses to the USER_EE_CTRL_1 register located at register address 0xA2 in page
0. Write ‘0x00’ to the register first to reset the unlock mechanism. The next
four writes must occur in order and no register accesses can be performed in
between the writes. First, 0x98, second, 0xB8, third, 0x13, and fourth 0x7D.
When the NVM has been successfully unlocked, both bits 6 and 7 of register
address 0xA3 in page 0 are set.Note: Register accesses include the
PFSM as well as the serial interface. During the unlocking of the NVM, the
PMIC must be in an idle state and the PFSM is not attempting to access the
register map. The MCU performing the unlock must also limit register
accesses to only those writes associated with the unlock sequence. In some
MCU serial communications an automatic readback of each register is
performed after each write. Any such mechanism must be turned off.
- Disable the PFSM
Once the NVM has been unlocked the next step is to
disable the PFSM. This is done by setting bit 0 of register address 0xA3 in page
0. Since this register also contains the contents of the unlock, write 0xC1 to
the register.
- Special Considerations for Buck
Frequency and Serial Interface Changes
After
disabling the PFSM and before writing the new content to the user registers any
special considerations for buck frequency or interface changes must be applied.
If the buck frequency remains the same and the serial interface is unchanged
then no additional instructions are required. See the applicable special
considerations as well as the example. Details are provided in Section 5.1 and Section 5.2
- Writing Content to pages 0, 1,
and 4
Writing to pages 0, 1, and 4 must only
include the register addresses described in Appendix A. In the event that the register CRC is enabled, then non-NVM registers must
also be returned to their default value as described in Appendix B.
- Writing Content to page 3
After completion of pages 0,1, and 4, write to
page 3. Page 3 is a special use case and requires additional handling to access
the sub-pages for the PFSM memory space. The page and sub-page
delineations can also be identified in the binary file, where page 0 is in the
address space 0x00-0xFF, page 1 is 0x100-0x1FF, page 4 is 0x400-0x4FF, and page
3, sub-page 0, is 0x3000-0x30FF, sub-page 1 is 0x3100-0x31FF, and sub-page 2 is
0x3200-0x32FF. A detailed description of the sub-pages is found in the PFSM section. Selecting the Page 3 sub-pages is done through
register 0xA4 on Page 0. CAUTION: The
TPS6594-Q1 and TPS6593-Q1 family of devices have three subpages for page 3.
The LP8764-Q1 device only has two subpages for page 3 and sub-page 2 does
not exist. Attempting to write to sub-page 2 of the LP8764-Q1 results in
writing to sub-page 1, corrupting the memory space.
Table 4-1 PFSM Address Control,
Register Address 0xA4, Page 0
| Bit |
Field |
Type |
Reset |
Description |
| 7-2 |
Reserved |
R/W |
0h |
|
| 1-0 |
PFSM_PAGE_SEL |
R/W |
0h |
Select the
Page 3 address space that can be addressed.
0:
0x000-0x0FF
1:
0x100-0x1FF
2:
0x200-0x2FF
|
- Lock the NVM to prevent future
programming (optional)
If locking the NVM to
prevent future updates is desired, then the value of register 0x41 on page 1
must be something other than 0xA5. Locking the NVM also prevents the ability to
access page 3 for validation purposes.Note: Locking the NVM is a
permanent decision and prohibits any future changes.
- Update register CRC
After all of the content has been updated in the
register map, then the register CRC can be calculated and applied. This is only
necessary if the register CRC is enabled in the NVM being configured.
- Move content from register map to
NVM
Now that all of the user register content
has been updated and the register CRC updated, the contents can be copied into
the NVM space. To initiate the transfer of content, set bit 1 of register 0xEF
in page 1. The transfer is not instantaneous and the status of the transfer can
be observed in bit 1 of register address 0xF3 in page 1. When this bit is
cleared then the transfer activity is complete.