SLYA051A october 2020 – april 2023 DRV5055 , DRV5055-Q1 , DRV5057 , DRV5057-Q1 , TMAG5170 , TMAG5170-Q1 , TMAG5170D-Q1 , TMAG5173-Q1 , TMAG5273
Based on the results from the preceding simulation, we can expect that the maximum appropriate sensor spacing is roughly the magnet length of 22 mm. This aligns with the maximum of one sensor with the minimum of the following device. In practice this presents a few challenges. Firstly, air gap, alignment, or sensitivity of the DRV5055 may vary enough to produce measurement gaps. Secondly, the output voltage is nonlinear near the extremes. This makes interpreting the final position difficult. As a result, it is recommended to have overlap between sensors.
Let us expand the previous setup and consider a linear array of 5 sensors with approximately 20 mm spacing between each sensor.
This spacing aligns the peak of one sensor with the linear output region of the adjacent sensor and gives us a total usable range of about 100 mm as shown in DRV5055 Output Response.
For the output data to be useful, it must be decoded. The system must decide which sensor output is most relevant at any given time to use for position calculations. An easy algorithm to determine which output should be monitored is as follows: