SNVU596A October 2018 – July 2025 LP87521-Q1 , LP87522-Q1 , LP87523-Q1 , LP87524-Q1 , LP87525-Q1
The nINT pin (pin 19) is an open-drain, active low output from the LP8752x-Q1 PMIC. Connect this pin to an external pullup resistor. If RESET_REG_MASK bit is unmasked, then an interrupt is generated on this pin whenever the RESET_REG_INT bit is set high. The RESET_REG_INT bit is set high when either the VANA supply voltage has decreased below the undervoltage threshold level or the host has requested a reset using the SW_RESET bit in the RESET register or device is reset by NRST. By monitoring the nINT pin, the MCU knows when the PMIC registers are reset to the default values determined by the OTP, and takes the necessary actions to make sure that the PMIC is configured as needed.
After a power-on reset, the LP8752x-Q1 PMIC requires a delay of 1.2ms before there can be any communication through the I2C interface. When the RESET_REG_MASK bit is unmasked, this required delay can be monitored through the nINT pin. After a power-on reset, the nINT pin is driven high while the registers are reset and the OTP is read to set the registers to their initial values. After 1.2ms, the nINT pin is driven low, signaling that the registers have been reset and can be configured to fit the design requirements.
Else, when RESET_REG_MASK bit is masked, nINT does not have any reaction to a power-on-reset.