SPRACX6 June 2021 DRA821U , DRA821U , DRA829J , DRA829J , DRA829V , DRA829V , TDA4VM , TDA4VM , TDA4VM-Q1 , TDA4VM-Q1
Attached in a zip file is an example modification done to SBL boot flow in Processors SDK 7.1, using the above sample code.
The sample code in the attached zip file is based on the Processor SDK memory map provided in Processor SDK 7.1. The firewall memory ranges would likely need to be customized for the platform under test.
To see the changes, the two directories in the zip file can be compared: