SPRAD05B May 2023 – December 2023 AM620-Q1 , AM623 , AM625 , AM625-Q1 , AM625SIP
The Hardware Design Guide for AM625, AM623, AM625SIP, AM625-Q1 and AM620-Q1 family of processors provides a starting point for the board designers designing with any processor of the family of processors. This hardware design guide provides an overview of the recommended design flow and design stages, and highlights important design aspects and requirements that must be addressed. Note that this document does not include all of the information required to complete the board design. In many cases, this document refers to the device-specific collaterals and various other user guide as sources for specific information.
This hardware design guide (document) is organized in a sequential manner. It starts from decisions that must be made during the initial planning stages of the board design, through the selection of key devices, electrical, and thermal requirements. For ensuring a successful board design, issues discussed in each of the section should be resolved before moving to the next section.
The hardware design guide is applicable to ALW, AMC and AMK package processors.
The hardware design guide may not cover every aspect of the board design.
These processor families have capabilities to address safety requirements.
The focus of the hardware design guide is non-safety applications.