SPRAD66B February 2023 – December 2024 AM62A1-Q1 , AM62A3 , AM62A3-Q1 , AM62A7 , AM62A7-Q1 , AM62D-Q1 , AM62P , AM62P-Q1
Figure 2-4 shows an example placement for the AM62Ax, AM62Px, AM62Dx processor and the LPDDR4 memory device. The recommended spacing parameters for the AM62Ax, AM62Px, AM62Dx device and the LPDDR4 device are defined in Table 2-3. The placement does not restrict the side of the PCB on which the devices are mounted. The ultimate purpose of the placement is to limit the maximum trace lengths and allow for proper routing space.
| Number | Parameter | MIN | MAX | UNIT |
|---|---|---|---|---|
| 1 | x1 | 1200 | Mils | |
| 2 | y1 | 250 | Mils |