SPRAD66B February 2023 – December 2024 AM62A1-Q1 , AM62A3 , AM62A3-Q1 , AM62A7 , AM62A7-Q1 , AM62D-Q1 , AM62P , AM62P-Q1
To achieve the high frequency targets of the LPDDR4 interfaces supported by the AM62Ax, AM62Px, AM62Dx family of devices, an excellent PCB implementation is required. TI highly recommends that customer designs copy the TI AM62A LP SK EVM or AM62P-LP SK EVM PCB layout exactly, and in every detail (PCB material, routing, spacing, vias, and so forth) to achieve the full specified interface frequency and data rate. If the design does not or cannot copy the TI design, then the EVM must still be used as a starting point, and simulations must be performed. The customer design can need to constrain the interface frequency and data rate based on the PCB implementation.
The goal of this document is to define a set of layout and routing and simulation rules that allow designers to successfully implement a robust design for the topologies that TI supports. This is also required that the PCB design be simulated to verify the design targets are achieved. TI limits debug and support for boards that have not been designed and simulated according to the steps defined in this document. Systems that do not follow the TI EVM implementation or do not have valid simulation results likely need to run at a reduced DDR frequency.
This document provides reference eye masks as guidance for validation of the simulations results. There is still an expectation that the PCB design work (design, layout, and fabrication) is performed and reviewed by a highly knowledgeable high-speed PCB designer. Problems such as impedance discontinuities when signals cross a split in a reference plane can be detected visually by those with the proper experience.
TI only supports board designs that follow the guidelines in this document. These guidelines are based on well-known transmission line properties for copper traces routed over a solid reference plane. Declaring insufficient PCB space does not allow routing guidelines to be discounted. TI limits debug and support for designs that have not been simulated according to the steps defined in this document.