SPRADB3 October 2023 AM2631 , AM2631-Q1 , AM2632 , AM2632-Q1 , AM2634 , AM2634-Q1 , AM263P4 , AM263P4-Q1
This application note describes the differences between the Texas Instruments AM263 and AM263P microcontrollers to provide details on the new features offered with AM263P and what needs to be considered when migrating from AM263 to AM263P. Both hardware and software changes are covered for the purpose of application migration. This document provides a comprehensive list of feature differences between the two devices. However, these details are kept at a feature level and specific information about the performance or usage of each feature should be found in the device-specific data sheets, technical reference manuals, or software user guides. Features that are identical between the devices are not included outside of the Device Comparison table.